{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a VeriSafe Absence of Voltage Tester (AVT) be used in Schneider Electric Model 6 Motor Control Centers?
Issue:
MCC buckets is it okay to install an AVT?

Product Line:
Motor Control Centers

Environment:
Application Assistance

Cause:
Unit compatibility and ordering

Resolution:
Yes, it is a standard application. VeriSafe AVT device allows tests to be administered with the MCC doors closed, with no exposure to potentially energized parts inside the MCC. VeriSafe ATV is a configurable option when building a new MCC, please reach out to your local distributor. For existing MCCs our field service department can handle this installation, reach out to Square D tech support for a quote. Click here to see the Model 6 MCC with VeriSafe Absence of Voltage Tester Handout file.

Schneider Electric Nigeria