{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How will Cyber security software blocking the Microsoft msxml4.dll component effect OFS?

The Microsoft component msxml4.dll is used for SOAP support.  Any version OFS 3.61 or lower will not run without this component.

OFS version 3.63 SP3 does not install this component because it does not support SOAP.

To resolve the issue, it is recommend to update OFS to version 3.63 SP3 or higher.

Schneider Electric Nigeria