{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Scan settings for Modbus devices with an ID above 247 in Data Center Expert can not be modified.
Issue:
Scan settings for Modbus devices with an ID above 247 in Data Center Expert can not be modified.

Product Line:
EcoStruxure Data Center Expert
StruxureWare Data Center Expert

Environment:
Data Center Expert versions 8.1.1 and below

Cause:
Although you can add a Modbus device with an ID up to 255, when editing device scan settings for Modbus devices, the dialog does not show any addresses above 247.

Resolution:
If you have discovered a device with an ID above 247 and need to modify it's scan settings, the only way to address this currently is to change the devices modbus ID to 247 or lower, delete the device from DCE, and re-discover it with the new ID

This issue is being looked into and there is currently no date or version set for this to be addressed.

Schneider Electric Nigeria