Yes you can FTP files out of the M340 PLCs via USB. The USB port is Ethernet like with a IP address of 90.0.0.1.
Gepubliceerd voor:Schneider Electric Netherlands


{}
Yes you can FTP files out of the M340 PLCs via USB. The USB port is Ethernet like with a IP address of 90.0.0.1.