{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Veelgestelde vragen (FAQ's) zoeken
Sepam display showing "Application not selected"
This issue is because of the application is missing in the cartridge (i.e. cartridge is blank) which is to identify the type of Sepam (e.g. T87, S80...etc).

There are 2 ways to solve this issue:

1. Return the Sepam relay back to replace to your local distributor or the company were you bought it.
2. Replace the cartridge with a new one which has a correct application inside.

Schneider Electric Netherlands

Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie