InRow Entering Fluid Temp threshold is not alarming
Issue:
InRow Entering Fluid Temp threshold is not alarming

Product line:
InRow

Environment:
Data Center Cooling

Cause:

Resolution:
In the newest firmware ACRC 372 and higher the entering fluid temp alarm threshold violation will not be reported unless two conditions are met. The unit has a >=40% valve position opening, and the entering temperature is above the threshold.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: