How to assign a logic input to freewheel stop on Altivar 61 and 71?
Issue:
Freewheel stop assignment on ATV61/71.

Product Line:
Altivar 61 and 71

Environment:
All models and serial numbers

Cause:
None

Resolution:
Go to Drive menu, 1.7 Application function menu, and assign Freewheel Stop assignment to a logic input (LIx) as desired.

NO.        MENU                              SUB-MENU        CODE   ADJUST    DESCRIPTION
1.7    APPLICATION FUNCTION    STOP CONFIG.    Nst      LIx            Freewheel stop input

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: