Where can I find a list of the ATV61 and ATV71 Communication Parameters?

Issue:
Is there a list of ATV61 and ATV71 Modbus registers available?

Product Line:
ATV61 and ATV71

Environment:
All models and serial numbers

Cause:
Modbus registers are unknown

Resolution:
ATV61 Communication Parameters manual: https://www.se.com/us/en/download/document/1760661/
ATV71 Communication Parameters manual: https://www.se.com/us/en/download/document/1755861/

See attached files in Excel Spreadsheet format as well.

Schneider Electric Norway

Vedlegg
ATV71_communication_parameters_EN_V5.7_IE67 (2).xlsx [187.17 KB]
atv61_communication_parameters_en_v5.8_ie29.xlsx [187.6 KB]
Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: