Are preset speeds active on the ATV212 when in local control?
Issue:
Can the preset speeds be used when ATV212 is in local control?

Product Line:
ALTIVAR 212

Environment:
All serial number

Cause:
N/A

Resolution
No, preset speeds are not active when in local control.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: