Can my SCADA system communicate to other Modbus Plus devices through the M340 Modbus Plus Proxy?
Issue
SCADA communication to Modbus Plus devices

Product Line
M340 Modbus Plus Proxy

Resolution
The M340 Modbus Plus proxy is used to communicate with the M340, M580, and Momentum PLC families.
For a SCADA system or another device to communicate with other Modbus Plus devices, a gateway would need to be used.
The Niobrara MEB II is the recommended gateway at this time.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: