Do any of the Altivar Drives have a Profinet option?

Issue:
Profinet option on ATV Drives

Product Line:
ATV61, ATV71, ATV32, ATV600, ATV900

Environment:
All

Cause:
Product Selection & Services

Resolution:
Yes, ATV600, ATV900, ATV320, ATV340, ATV61, ATV71, and ATV32 offer options cards that support Profinet.
​ATV600/ATV900/ATV320/ATV340/ATV32 Profinet option card part number VW3A3627.
ATV61 / ATV71 Profinet option card part number VW3A3327.
Some older version drives may not support the Profinet option card. Be sure to verify compatibility before ordering.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: