Can 5506 module, eight analog inputs, detect that wire/connection to 4-20mA sensor is broken?
Yes! The module returns status information for each analog input indicating if the analog input is in or out of range for the defined signal type. When analog input is configured for 4-20mA and wire is broken (input current 0mA) status bit associated analog input will be turned ON!

Schneider Electric Norway