Does Schneider Electric offer the Berger Lahr EXRDM3913/50NEA motor or a suitable replacement?
No, the Berger Lahr EXRDM3913/50NEA motor with ID number 52951045500 is a special customized version for the company W&H (Windmoeller & Hoelscher)
This motor type is proprietary and is reserved for the company W & H and cannot be purchased from Schneider Electric.
Customers must contact the OEM machine builder Windmoeller & Hoelscher for a spares or replacements.


rev 10-2-18

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: