Do the CSH120 and CSH200 CTs work with VAMP relays?
Product Line
VAMP

Resolution
Yes, the CSH120 and CSH200 core balance CTs will work on the VAMP relays so long as the CT inputs are the 1A / 0.2A input option.

Note:  See attachment for instructions on using the CSH CT's with the VAMP relays.

Schneider Electric Norway

Vedlegg
Using-CSH120-with-VAMP-protection-relay-range.pdf [115.55 KB]