Does the ATV340 have programmable logic functions like the ATV32 and ATV320?

Article available in these languages: Spansk

Issue:
Wondering if the ATV340 drives have programmable logic functions, like the ATV32 and ATV320?

Product Line:
ATV 340

Environment:
All

Cause:
Configuration

Resolution:
The ATV32 and ATV320 have logic functions that you can program via SoMove.  The ATV340 is configured like the ATV630 and the ATV930, so the answer is No, there is no internal logic.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: