Video: What is the part number of compact display module to be used with TeSys T LTMR controllers?
Issue:
Connecting LTMCU Compact Display for TeSys T LTMR Controllers

Product Line:
TeSys T, LTMR

Environment:
LTMR Controllers

Resolution:
The part number is LTMCU.  With this you can configure parameters, display information, monitor alarms and detected faults, local control of motor, and select different languages as defined by documentation.

It requires an RJ45 connection cable to connect the keypad to the TeSys T module/expansion.

Connecting to a TeSys T LTMCU HMI Device

TeSys T LTMCU HMI video

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: