Vista diagram was configured to include alphanumeric objects that use a timestamped display, however when the diagram is viewed in Diagrams the timestamp is not shown, only the value.
Product Line
Power Monitoring Expert 9.0

Environment
New installs or upgrades to Power Monitoring Expert 9.0

Resolution

Cumulative Update 2 (CU2) should be applied to the system to fix this issue.

The download for CU2 can be found here: FA380714

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Kategori:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde:
Kategori: