What is the electrical specifications for the status output state on a XPSMCMCP0802 Safety controller?
Issue:
Information on the status output state of a XPSMCMCP0802 safety  PLC.

Product Line:
XPS safety PLC line

Environment:
SOSAFE Configurable

Cause:
Documentation for the specifications on the status output.

Resolution:
The test output state for the short circuit overload maximum current is 100 ma at 24vdc.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: