ION8650 switchboard case dimensions
Issue
Dimensions of ION8650 switchboard meter case in 3D CAD file does not match the dimensions mentioned in the installation guide

Product Line
ION8650 Switchboard

Environment
Mechanical Dimensions

Cause
The dimensions showing in installation guide is misleading

Resolution

ION8650 switchboard meter installation guide indicates that the dimension of the switchboard case is 286 mm in height as shown in the diagram below.

ION8650 switchboard case dimensions

This dimension is incorrect. The dimension in question should be 267mm, there is a difference of 1mm between the correct dimension (i.e 267 mm) and the 3D CAD file (266mm) due to a small piece that is on the diagram and not included in the 3D model. The technical publications group has been notified of the difference, we don't have a publication date for the updated documents(installation guide and 3D files).

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: