Can we display the actual real time value on a Trend Graph?
Issue:
Looking for a way to display the actual values recorded on the Real Time Trend.

Product Line:
Vijeo Designer (all versions)

Resolution:
Currently it is not possible to display the actual values of the recorded data points on the Real Time Trend Graph. The workaround solution is to use the Historical Trend Graph and press the back/forward button to traverse the graph. It will show the data value as it passes through each data point on the right hand side of the graph.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: