Power Monitoring Expert - printing web page from Diagrams can produce unreadable output
Issue
Trying to print diagrams page directly from the browser in Web App produce unreadable output.
Product Line
Power Monitoring 9.0
Power Monitoring 2020

Envoriment
Web Application - Diagrams

​​​​​​Cause
The print page does not print well formatted because it includes information about what the Grouping Window is set to do.

Resolution
The workaround suggested for this issue is to take screen captures of the pages and print.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: