Can I use the Unity Loader utility to upgrade the firmware of the BMENUA0100 OPC UA module?

Issue:
Utility used for upgrading the firmware of the BMENUA0100 OPC UA module


Product Line:
M580, EcoStruxure Control Expert, BMENUA0100


Resolution:
No, The Unity Loader cannot be used for upgrading the firmware of the OPC UA module. You must use the EcoStruxure Automation Device Maintenance V2.0 utility. You can download the utility and firmware file from the Schneider Electric public site at

EcoStruxure Automation Device Maintenance V2.0 :
https://www.se.com/ww/en/download/document/EADM/

BMENUA0100 OPC UA module firmware:
https://www.se.com/ww/en/search/bmenua0100?multifilter=Software

Schneider Electric Norway

Finn ut mer
Produkt:
Artikler som kan være nyttige
Finn ut mer
Produkt: