Why does the connection status LED stay gray when updating the ATV930 or ATV630 Drives firmware using the EADM software tool?

Issue:

What do the status LED colors mean when updating the Process Drives firmware using the EADM software tool?

Product Line:

EADM tool with ATV630, ATV930 or ATV340

Environment:

All

Cause:

Status indicator LED meaning

Resolution:

There are three colors for the status:

-    Green – Drive reachable and logged-in

-    Yellow – Drive reachable and not logged-in

-    Gray – Drive not reachable (drive power off / disconnected)

EADM file 1

EADM file 2

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: