{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between 22mm contact blocks ZBE101, ZBE1016, and ZBE1016P?
Issue:
ZBE101, ZBE1016, and ZBE1016P differences

Product Line:
Harmony Push Buttons

Environment:
Harmony 22mm

Resolution:
The ZBE101 has silver contacts, ZBE1016 is gold plated, and ZBE1016P is both gold plated and has dust protection, with a sealed plastic casing.

Schneider Electric New Zealand

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.