{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number and function of the remote racking devices for Masterpact NT and NW?
Product Line:
Circuit Breakers
Masterpact NT and NW
Remote Racking

Environment:
Electrical Distribution Equipment

Resolution:
The Masterpact NTMPRRT and NWMPRRT Remote Racking Devices are intended to allow remote insertion and removal of a Masterpact NT or NW circuit breaker from its chassis, and racking between the disconnected position and the connected position. Operation can be performed from outside the arc flash zone as described by NFPA 70E/CSA Z462.


Schneider Electric New Zealand