{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What temperature (how hot) can the external enclosure surface of Low Voltage Transformers reach?

Article available in these languages: Spanish

Issue:
The temperature reached by an Energized Enclosed Transformer can be an important quantity, as it contributes heat to the surrounding environment
Product Line:
LV Transformers
Environment:
Applies to Ventilated Transformers and Sealed Resin Epoxy Encapsulated Transformers
Cause:
Energized Enclosed Transformers generate heat which is transmitted to the surface of the Enclosure
Resolution:
Underwriters Laboratories standards limit the external surface temperature of transformer enclosures to 50ºC (90ºF) rise above ambient for both ventilated and non-ventilated enclosures and 65ºC (117ºF) rise above ambient for epoxy resin-filled transformers. Since the transformer core loss is present even under no-load, some parts of the enclosure will come near this limit even under the condition of light loading, or even no-load. In a typical ambient of 25ºC (77ºF) it is not unusual for the outside surface at the top of a ventilated transformer to reach 70ºC (158ºF) with no load on the transformer. Epoxy resin transformer enclosures can reach even higher temperatures approaching 85ºC (185ºF) even at no-load.


Schneider Electric New Zealand