Search FAQs
How do I swap my Wiser connected switch and dimmer devices from BLE to Zigbee?
To swap from Bluetooth to Zigbee you will need to short press the mechanism 12 times - and allow time for the device to swap modes, this will take roughly 40 seconds. Initially when swapped to Zigbee mode the LED indicator on the mechanism will flash amber indicating it is in pairing mode. If not paired to after roughly 50 seconds this will become solid amber. This amber indicator will remain on until paired with a Hub, the mechanism will function as normal while this indicator is on.
NOTE: Before swapping from Bluetooth/BLE to Zigbee it is strongly recommended that a factory reset be performed on the mechanism before initiating the change.
NOTE: Before swapping from Bluetooth/BLE to Zigbee it is strongly recommended that a factory reset be performed on the mechanism before initiating the change.
Released for:Schneider Electric New Zealand
Explore more
Product:
Explore more
Product: