If your roller door can have a wired switch installed to operate it, you can use the Micro Module Switch CLP5011WSZ. It requires an active and neutral to operate but has dry contact that can be used in conjunction with wiring from the roller door. Once installed a 1 second timer will have to be implemented by programming a simple Automation in Wiser by SE to create a ‘pulse’ connection similar to how a bell press or momentary switch would operate.
It also requires that all wiring be 240V cabling, installed with proper electrical workmanship by a licensed electrician. Ensuring all terminations, cables and the CLP5011WSZ are restrained and supported correctly.
It also requires that all wiring be 240V cabling, installed with proper electrical workmanship by a licensed electrician. Ensuring all terminations, cables and the CLP5011WSZ are restrained and supported correctly.
Released for:Schneider Electric New Zealand