Search FAQs
I want to put in two-way switching but can’t run the cables between the mechanisms. Can I achieve wireless two-way switching with Wiser Zigbee?
This can be done with our 2AX, 10AX or Micro Module Switch along with the Hub. At one end you will need an Active, Neutral and Load wiring. At the other end you will need Active and Neutral only. You can then create Automations to achieve the 2-way.
You need to create two automations for a 2-way:
You need to create two automations for a 2-way:
- when switch A and switch B are ON, turn switch A and switch B ON
- when switch A and switch B are OFF, turn switch A and switch B OFF
This can be expanded to 3-way, 4-way etc by simply adding the other switches into the respective ON and OFF automations.
Released for:Schneider Electric New Zealand
Explore more
Product:
Explore more
Product: