Search FAQs
My Wiser battery device is showing the battery is almost flat, can I replace the battery and what do I replace it with?
All battery devices in the Wiser range have pictograms on how to change the battery in the instructions, which are available on the appropriate product page on our website (https://www.clipsal.com/products/wiser-smart-home-solutions). It also states the type of battery used for each unit.
CLP591011/PDL591011 - Window/Door Sensor - CR2450 x 1
CLP595011/PDL595011 - Motion Sensor - LR03 AAA x 2
CLP593011/PDL593011 - Temp/Humidity Sensor - CR2450 x 1
CLP592011/PDL592011 - Water Leakage Sensor - LR03 AAA x 2
CLP591011/PDL591011 - Window/Door Sensor - CR2450 x 1
CLP595011/PDL595011 - Motion Sensor - LR03 AAA x 2
CLP593011/PDL593011 - Temp/Humidity Sensor - CR2450 x 1
CLP592011/PDL592011 - Water Leakage Sensor - LR03 AAA x 2
Released for:Schneider Electric New Zealand
Explore more
Product:
Explore more
Product: