To access a Connexium switch, you can use two methods :
Accessing Connexium through Browser Webpage
Requirement:
-
Connect to the switch: Use an Ethernet cable to connect your computer or laptop to one of the Ethernet ports on the Connexium switch.
-
Configure your computer: Set your computer's IP address to be in the same subnet as the default IP address of the Connexium switch. For example, if the default IP address of the switch is 192.168.0.1, set your computer's IP address to something like 192.168.0.2.
Accessing Connexium through Browser Webpage
Requirement:
- Edge browser in Internet Explorer mode
- Follow the setup here for Edge Internet Explorer mode in Microsoft Edge
- Add the IP address to IE Mode Page
- Java Version 8 (build 1.8.0_321-b07)
- Install jre-8u202-windows-i586.exe
- Navigate to the Control Panel section and select JAVA
- Under the Security Tab Select the following setting and add the IP address to the Exception List.
Accessing Connexium through Schneider Electric Viewer
Download and install Schneider Electric Viewer 3.2
Run the Software and add the IP Address in the URL Section
Download and install Schneider Electric Viewer 3.2
Run the Software and add the IP Address in the URL Section
Released for:Schneider Electric New Zealand