{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

What does the 's' on the Power Meter Accuracy class 0.2s & 0.5s mean?

It refers to the accuracy of the meter. A 0.2s meter has a much higher accuracy as below. Since Accuracy depends on the load of the system, IEC/AS have developed different standards to define...

How hot can circuit breakers get? What is the temperature of a molded...

Issue: What is the temperature of a molded case breaker? Product Line: Circuit Breakers Resolution: The acceptable operating temperature of a circuit breaker is defined by UL in the UL489 standard...

What is the replacement for the LA2-D22-A65

It will be the LADT2 and is only compatible with the TeSys D and TeSys F range.

Why does the ION Meter read negative kVAR?

When your ION Meter is reading negative kVAR, kindly check the Power factor value on the meter. If the power factor is leading and you have Capacitive load, it is possible to have negative kVAR...

What is a current limiting circuit breaker?

Issue: What is a current limiting circuit breaker? Product Line: Molded Case Breaker, Powerpact Resolution: A current limiting circuit breaker is one that has been certified by UL to limit the...

What is the difference between A9D32620 and A9D33620 RCBO Acti 9 devices?

A9D33620 = SI (Super Immunised) A9D32620 = Type A (AC or pulsating DC) Type A RCBO = Tripping is ensured for residual sinusoidal alternating currents and residual pulsating direct currents, whether...

What is the complete RJ45 connector pinout for ATV320?

The complete pinout, Pin 1 = CAN_H Pin 2 = CAN_L Pin 3 = CAN_GND Pin 4 = DI Modbus Signal Pin 5 = DO Modbus Signal Pin 6 - Not connected Pin 7 = VP, 10Vdc Pin 8 = Common The CANopen signals on the...

How can I connect SoMove to an Altivar Process drive via Ethernet TCP/IP...

Issue: Connecting SoMove to the VFD using the Ethernet network connection. Product Line: ATV61 ATV71 ATV630 ATV930 ATV320 ATV340 ATV32 Environment: Ethernet IP or Profinet option installed. VW3A3316,...

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What is Modbus and How does it work?

What is Modbus? Modbus is a serial communication protocol developed by Modicon published by Modicon® in 1979 for use with its programmable logic controllers (PLCs). In simple terms, it is a method...

Why choose Type B RCD for 3 Phase Variable Speed Drives?

For the 3 Phase Variable Speed Drives, the RCD type B or type B-Si is particularly suitable. It protects against fault currents with DC offset, which is true for three-phase power converters. In...

Apa alternatif replacement battery UPS SURT15KRMXLI jika APCRBC140 tidak...

Apa alternatif replacement battery UPS SURT15KRMXLI jika APCRBC140 tidak ready stock? ======================================================================= Untuk alternatifnya bisa menggunakan...

How to lodge warranty claims to Schneider Electric Australia for Schneider...

Go to the SE Solar - Get Support website https://solar.schneider-electric.com/netsuite/ Fill in all mandatory fields, upload a scan of proof of purchase (customer invoice), supporting photos, single...

What are the effects of dV/dt on a Motor when using a VSD?

As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on...

How do I access the Tools Page in eDLT

Press and hold down the bottom left button, whilst continuing to hold then double press the top right button. Please note that access to the Tools Page can be disabled using C-Bus Toolkit software.

What are the ranges of the Square D Circuit Breakers?

Material Description Comment Direct Replacement QO106EC10 MINIATURE CIRCUIT BREAKER 240V 6A Discontinued no replacement QO110EC10 QOvs 1P 10A 10kA Type C Direct Replacement QO110VSC10 QO116EC10 QOvs...

Can I use a 15A socket with a 10A plug?

Yes, a 15A socket with a 10A plug will fit.

Show more