How is the OPR parameter scaled on the ATV71 series drive?

Article available in these languages: Espanhol

Issue:
Scaling the Analog Output when using Output Power on an ATV61/71.

Product Line:
ATV61/ATV71

Environment:
All models, All serial numbers

Cause:
N/A

Resolution:
The output power (OPR) function is scaled between 0 and 2.5X the NPR (Rated motor power) setting under menu 1.1 (Simply Start).   This parameter should be set to match the horsepower or KW rating of your motor in order for the output scaling to be accurate.

Schneider Electric Portugal

Explorar mais
Gama:
Artigos que possam ser úteis
Explorar mais
Gama: