Pesquisar nas perguntas frequentes (FAQ)
What are the Hot Fixes for Unity Pro v11.0 to configure the PRM with M580?
Issue
This resolution clarifies the minimum hot fixes to be installed in Unity Pro v11.0 that guarantee a correct value of the variables from the PRM.
Product Line
EcoStruxure Control Expert, M580, PRM (TCSEGPA23F14F)
Environment
Unity Pro v11.0, BMEP581020 v2.50, PRM
Resolution
The PROFIBUS Remote Master (PRM) is a Profibus gateway that can also be used with M580 and the variables of the slaves are populated by a Device Derived Data Type. So, you need to install the hot fixes below to have a right order of bytes on Device DDT variables of the module and also when you connect the PRM to the BMENOC0301/0311/0321, modify the subnet mask or gateway address in the DHCP server:
- UnityPro_V110_HF0312464R_P-V81-M580 PRM data in DDT are mixed
- UnityPro_V110_HF0325873R DTM BMENOC doesn't transmit configuration to DTM PRM