{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you replace the overloads on the GV2, GV3 or GV7 starters?

Issue:
Are the bimetallic units in the GV starters replaceable?

Product Line:
IEC Contactors and Starters

Environment:
GV Manual Starters and Protectors

Cause:
Maintenance

Resolution:
The overload bimetal elements are not replaceable on these type starters, replace the complete unit only.

Schneider Electric Saudi Arabia