Issue:
The high horsepower Altivar 58, with software version V5.1 gives a INI fault on a V4.1 keypad display.
Product Line:
ATV58
Environment:
Keypad
Cause:
n/a
Resolution:
The high HP ATV58 drives require the use of V5.1 keypads. They will not work with earlier version keypads and will cause this error. Note the compatibility chart, in the beginning of the ATV58 keypad programming manual. These keypads have been obsoleted and are no longer available.
The high horsepower Altivar 58, with software version V5.1 gives a INI fault on a V4.1 keypad display.
Product Line:
ATV58
Environment:
Keypad
Cause:
n/a
Resolution:
The high HP ATV58 drives require the use of V5.1 keypads. They will not work with earlier version keypads and will cause this error. Note the compatibility chart, in the beginning of the ATV58 keypad programming manual. These keypads have been obsoleted and are no longer available.
Released for:Schneider Electric Saudi Arabia