{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can an LRD overload relay be used on a DC system ?

Issue:
DC Motor overload protection

Product Line:
Tesys D contactors

Environment:
Products sold and used in the United States

Cause:
LRD overload relay used in a DC power circuit

Resolution:

Yes, this is fine below 300vdc, simply series connect the poles or use an LR3D overload relay without single phase sensitivity.
Please note while the Tesys D contactors are suitable, they are not UL listed for DC power circuits.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: