Issue:
Settings and parameters saved in the drive or keypad.
Product Line:
Altivar 58
Environment:
All
Cause:
N/A
Resolution:
The actual program that the drive uses to run is stored in the drive control board itself. Removal of the keypad will not alter that program.
NOTE: There is storage memory available in the keypad that can be used to save a copy of the parameter settings. This may not be the same as the actual program that the drive is using.
Settings and parameters saved in the drive or keypad.
Product Line:
Altivar 58
Environment:
All
Cause:
N/A
Resolution:
The actual program that the drive uses to run is stored in the drive control board itself. Removal of the keypad will not alter that program.
NOTE: There is storage memory available in the keypad that can be used to save a copy of the parameter settings. This may not be the same as the actual program that the drive is using.
Released for:Schneider Electric Saudi Arabia