{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Will the current version of Power Suite Software work with older ATV58 drives?

Issue:
N/A

Product Line:
Altivar Machines, Altivar 58

Environment:
All

Cause:
N/A

Resolution:
Yes, the current version should be able to set any setting in your existing drive.

It will not be possible to use features that are available in the software that are not part of the drive.
For example, one could not assign a logic input to an external fault contact on a drive with version 4.1 firmware. It may show up as an option on Powersuite, but it is not a feature that was available with version 4.1 or older drives.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: