{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement keyed operator for the XB3D cam switch?
Issue:
XB3D keyed operator broke

Product Line:
Push Buttons and Operator Interface

Environment:
Cam switches Harmony Pushbuttons

Resolution:
No replacement parts are available for the XB3D cam switches.  These were custom built as a complete device only.

NOTE the XB3D are obsolete with no direct replacement.  Consider the 9003K2 cam switch product line.  See attached file.

Schneider Electric Saudi Arabia

Attachment(s)
9003CT1301R0616 Cam K2.pdf [1.43 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.