{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What will cause a OHF fault on the ATV58?

Issue :
OHF or overheat fault on the ATV58.

Product Line :
Altivar 58

Environment :
All

Resolution :
This fault indicates overtemperature of the drive.
Check the motor load, cooling fan(s) and the ambient temperature of the drive.
Make sure that the heatsink is clean and that there is nothing obstructing the air flow past the heatsink.
It is best for the drive to be mounted with the heatsink against a flat surface. The drive should be mounted in a vertical position. This allows for proper convection cooling.
Once the drive cools down the unit will restart.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.