{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATS48 control module have conformal coating on it?
Issue:
Coating on ATS48 control module.

Product Line:

Altistart 48


Environment:

All

Cause:

Altistart 48 Control Module

Resolution:
There is some degree of conformal coating.  The specification on the unit for Maximum ambient pollution is that it conforms to IEC 60664-1, Pollution Degree 3.





Schneider Electric Saudi Arabia