{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a 9001 KA contact block that is rated 6A at 125VDC?

Issue:
9001KA contact rating

Product Line:
9001 Type K Heavy Duty Operators

Environment:
30 mm Push Buttons

Resolution:
No., the 9001KA contact blocks have a maximum of 2.5A continuous at 125VDC.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: