{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the SR2A101FU be programmed from the front of the relay without using the PC and software?
Issue:
Programming a Zelio SR2 without a PC

Product line:
Zelio IEC Style Smart Relays

Environment:
Relays and Timers

Resolution:
Yes it can, but it has to be in LADDER language only.

Schneider Electric Saudi Arabia