{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the S316 suffix mean on the ATS48 soft starter?
Issue:
ATS48 part number ends with S316.  What does this mean?

Product Line:
ATS48

Environment:
S316

Cause:
n/a

Resolution:
This is a special version of the ATS48 designed to take advantage of a situation where a customer has a 6 or 12 lead delta wound motor (common in the hydraulic elevator market).  This soft start is uniquely wired into the windings of the motor (hence the need for 6 or 12 motor leads), in order to multiply the HP capability of the soft start. This is sometimes called inside Delta wiring.

The control card VX4G481 is common for all the soft starter including S316. The specification S316 is on the power board. To place an order for the power board, add S316 suffix. For example: VX5G48C32YS316.

NOTE: The S316 product is not stocked and is not normally available in the US.

Schneider Electric Saudi Arabia

Attachment(s)
FA109945.png [115.25 KB]