{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between ZB4 and ZB5 pushbutton offers?
Issue:
What is the difference between ZB4 and ZB5 lines?

Product Line:
22mm, Harmony Push Buttons

Environment:
Harmony 22mm

Resolution:
The ZB4/XB4 series have metal operators and mounting collars.  The ZB5/XB5 has plastic operators and mounting collars.

Both lines use the same contact blocks, light modules and accessories.  Just the collars and heads are different.  The mounting collar for the metal line is ZB4BZ009 and ZB5AZ009 for the plastic collar.  The operators and collars are not interchangeable between plastic and metal.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.