{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the latch bar rivets for the Class 9423 Type M door closing mechanisms?
Issue:
Latch Bar Rivets for the Class 9423M3, M4, M9, M23 and M24.

Product Line:
Operating Mechanisms,Disconnect Switches, and Door-Closing Mechanisms

Environment:
9423 Door-Closing Mechanisms

Resolution:
The door closing mechanisms are supplied with the 31008-124-01 rivet(s) as standard. For replacement purposes order as outlined below:

9423M3 and 9423M23; requires (1) 31008-124-01 rivet.
9423M4, 9423M9 & 9423M24; requires (2) 31008-124-01 rivets.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: