{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement coil cover for 8536SC** starter?
Issue:
What is the replacement coil cover for 8536SC** starter?  ** is followed by (1) letter (enclosure type) and (1) or (2) numbers - For example - 8536SCG3, 8536SAG12, etc.

Product Line:
8502, 8536 Nema Type S Starter

Environment:
8502, 8536 Nema Type S Starter

Resolution:
31127-013-01 is the cover only.
The cover is secured by (2x) 21937-14341 mounting screws. Cover does not include nameplate and the nameplate not available for safety reasons.

NOTE: 31127-013-01 is no longer available

Schneider Electric Saudi Arabia