{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which ATV71 encoder card would be used with a differential line driver encoder?
Issue:
ATV71 encoder card used with a differential line driver encoder

Product Line:
Altivar 71, ATV71

Environment:
All

Cause:
N/A

Resolution:
The RS422 Encoder interface card would be used.
If required 5v, it would be VW3A3401.
If required 15v, it would be VW3A3402.

Schneider Electric Saudi Arabia