{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the operating time be reset to zero on the Altistart ATS48?
Issue:
Needs to reset the operating time to zero on the ATS48.

Product line:
Altistart 48, softstart

Environment:
all

Cause:
Reset operating time

Resolution:
Yes.  Can go into the dRc menu and in the rPr parameter:  The options available here are:

- no: function inactive
- APH: kWh reset to zero
- trE: operating time reset to zero

The reset command must be confirmed with ENT. APH and trE take effect immediately.
The parameter then automatically returns to no.

Schneider Electric Saudi Arabia